9/26/2017 5:38 AM | |
Posts: 9 Rating: (0) |
I edited a node red-modbus stream, modbus-getter set to serial mode, when clicked on the deployment, the server will crash, display illegal instructions。 |
10/17/2017 5:01 AM | |
Posts: 9 Rating: (0) |
I am using the latest version v0.17.5 |
10/31/2017 1:12 PM | |
Posts: 7 Rating: (0) |
I have the same issue, also i found this and it did not work: [code] Illegal InstructionThe pre-compiled binaries assume a fully capable chip. Intel'sGalileo 2, for example, lacks a few instruction sets from the #Will ask npm to build serialport during install time npm install serialport --build-from-source #If you have a package that depends on serialport, you can ask npm to rebuild it specifically... npm rebuild serialport --build-from-source [/code] |
11/9/2017 11:01 AM | |
Joined: 9/2/2013 Last visit: 11/6/2020 Posts: 48 Rating: (19) |
Look here: |
11/29/2017 2:09 PM | |
Joined: 6/19/2017 Last visit: 5/6/2024 Posts: 7995 Rating: (163) |
New question published by eric00058 is split to a separate thread with the subject Node-red-node-serialport on an embedded liniux 4.4.18 yocto platform. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on