10/27/2017 10:06 AM | |
Posts: 6 Rating:
|
Is it possible for someone to ellaborate on the connection of logo! AM2 with the logo! 230 RC? (possibly with a wiring diagram) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/30/2017 9:05:04 AMNew subject after splitting |
|
10/27/2017 4:34 PM | |
Joined: 12/18/2014 Last visit: 8/25/2024 Posts: 33616 Rating:
|
We like to help. But good help can only be provided with good information from questioners. All expansion modules are connected to the base module or another expansion module in the same way (see attachment). To generate a voltage of 0-10V for an analog input with a potentiometer: You make a series circuit consisting of a 6.6 kΩ resistor and a 5 kΩ potentiometer. Connect the other side of the 6.6 kΩ resistor with the plus of the 24 VDC power supply of the AM2, the other end of the potentiometer with the M of the voltage supply. AttachmentLOGO! 8 Soft manual 0BA8 2016_07 (FS4) pages 36-37.pdf (442 Downloads) |
10/27/2017 5:03 PM | |
Posts: 6 Rating:
|
Thank you for the invaluable help. |
This contribution was helpful to
1 thankful Users |
Follow us on