10/28/2017 7:12 AM | |
Posts: 6 Rating: (0) |
Dear All, I can not establish communication between STEP5 from my laptop, and Sinumerik 810t GA3 CNC. My laptop has DB 9 RS232 COM1 port. I used a standard V24 serial cable, with which I can communicate very well with CNC control by WinPCIN software. I have downloaded PLC program in binary format (%PCP file), but I can not open this file with STEP5. When I try to go ONLINE with STEP5, after I have set machine bits 5010 and 5011(communication parameters) accordingly , I get the message "PLC time out" on STEP5. For STEP5 is necessary another cable? On the Installation manual of the Sinumerik, the list of devices which can be linked with the CNC contain only PG programmers, not also STEP5 on the PCs. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/30/2017 9:18:31 AMNew subject after splitting |
|
10/28/2017 9:15 AM | |
Posts: 92 Rating: (5) |
Hi there set the controllers baud rate to 9600, your connection is not correct. |
10/29/2017 6:30 PM | |
Posts: 92 Rating: (5) |
Dear vs60 Its good to hear that you reload your controller. you need to set some setting on the control system and "axual" (Working area sett and sometimes a parameter) to run your machine. It's Ok. If you want to edit ladder file on S5, you need to reload your controller and take a backup from S5. please tell me about the Version of your Operation system and PC, also S5 connection is sensible, don't use USB, Remove PCI cards if you can, sometimes you need to turn off the Anti-Virus and close the other programs, noise is matter. 5010/5012: 00000100 5011/5013: 11000111 5016:00000000 take a look at the attached file. Attachment810T_GA1_Step5_v72.pdf (497 Downloads) |
7/27/2018 12:19 AM | |
Joined: 3/4/2011 Last visit: 2/12/2021 Posts: 2 Rating: (0) |
Dear vs60, Did you solve your problem, may be i can help |
Follow us on