11/1/2017 10:49 AM | |
Joined: 11/1/2017 Last visit: 3/28/2024 Posts: 1 Rating: (0) |
Hello to all.. I am working on a SNMP OPC Server trying to read some tags from Scalance Switches over the IE network. I have already configured my Server as Simatic PC Station with Step7, creating with this way a OPC Server module and IE General in it like the manuals say. Also, i configured the SNMP over the edit plant configuration adding the switches there i would like to monitor over the OPC. Now, i am using the OPC Scout V10 and over the Local Server i have NO TAGS in SNMP Subfolder. Any Suggests? Thanks. AttachmentSNMP_config_PC_Station.pdf (583 Downloads) |
11/30/2017 12:48 PM | |
Joined: 9/3/2008 Last visit: 5/24/2024 Posts: 922 Rating: (158) |
Hi, After configuration in Edit Plant and then download to Station Configuration Editor, there should be devices in the snmp folder. See the attached printscreens as example. Attachmentsnmp-config.zip (417 Downloads) |
Michael |
|
Follow us on