11/9/2017 10:09 AM | |
Posts: 5 Rating: (0) |
Dear All, i have a redundant system consisting of two cpu's (412-5H PN/DP) , using step 7 v 5.5, connected with Sematic HMI winCC comfort/ advanced v 13.0 & step 7 prof. v 13.0(TIA portal) via industrial Ethernet network . Now i would like to add two CP's 443-1 to the network in order to perform the same tasks. My questions are: 1- how to configure/set-up those CP's ? 2- which FB's/FC's do i need to add into the user program to ensure communication between each cpu and CP? 3- do i need to include any communication software (like ModBus_TCP_red...library) to ensure redundant functionality of the system? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 11/9/2017 7:19:51 PMNew subject after splitting |
|
Follow us on