11/20/2017 10:22 AM | |
Joined: 7/5/2015 Last visit: 4/29/2024 Posts: 19 Rating: (0) |
hello, I'm facing a problem to upload program from CPU 317-2PN/DP by PC Adapter USB A2. when a try to upload the program a message has came. the message screenshot is given on attached file. i have select PG/PC Interface PC Adapter Profibus and MPI both. the same message has came in both PG/PC interface. please give me the solution. Regrads Apon ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/20/2017 2:33:13 PMNew subject after splitting |
|
11/20/2017 12:02 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi, this is usually an adress-conflict in MPI-adresses. But there can be an other cause: The reason for this can be an actual fault in the hardware, or an interrupt conflict with another module. remedy: In this case the customer can check whether the MPI LED on the CP5611 from "What is the meaning of the error codes (xxxx:yyyy) in STEP 7?" hope this helps, regards, |
Last edited by: mopS04 at: 11/20/2017 12:03:41 PMFCK WAR! |
|
11/20/2017 12:38 PM | |
Joined: 7/5/2015 Last visit: 4/29/2024 Posts: 19 Rating: (0) |
how can i find the right baud rate? and which baud rate is suitable for 317-2PN/DP? |
11/21/2017 8:18 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hi, and what is shown in accessible nodes? Regards Christoph |
Follow us on