1/4/2018 4:13 PM | |
Joined: 9/23/2005 Last visit: 6/11/2024 Posts: 4346 Rating: (1433)
|
As from TIA V15 it is possible to monitor a V14 project running in a CPU. Requirements: The CPU should have a V14 (or superior) program version, without safety blocks. The a converted to V15 project version should be opened in TIA V15 TIP: In the project tree will show an special sign to indicate that the monitored project stay in a different version of TIA. It is possible to make changes in RUN, but the CPU project is actualized to V15 version in this process.\ The attached cast demonstrates this feature.Attachmentonline.zip (477 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to5 thankful Users |
Follow us on