1/21/2018 2:35 PM | |
Joined: 4/28/2015 Last visit: 8/3/2024 Posts: 58 Rating: (2) |
Thanks ORECA, Is it possible to use FB51 in STEP5 (no PCS7) ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/22/2018 10:47:34 AMNew subject after splitting |
|
1/22/2018 1:21 PM | |
Joined: 10/16/2007 Last visit: 9/11/2024 Posts: 629 Rating: (45) |
What is this FB51 for? Where is it from? |
1/25/2018 6:45 AM | |
Joined: 10/24/2011 Last visit: 6/23/2024 Posts: 71 Rating: (4) |
Hi Oreca, maybe I have one idea for you. I cannot use FB51, because I use S5 CPU with HMI panel OP7 and in my case FB51 is one of system communication blocks for communication CPU S5 and OP7. J |
1/26/2018 12:44 PM | |
Joined: 10/16/2007 Last visit: 9/11/2024 Posts: 629 Rating: (45) |
Just rename the FB51 which is not for the communication with the panel. Regards |
Follow us on