1/31/2018 11:25 AM | |
Joined: 1/26/2007 Last visit: 8/27/2024 Posts: 123 Rating: (4) |
hello, I am using Im151-8Pn and 7 distributed profinet IO(IM151-3PN). Complete program is made in TIA V14 i need to put alarms on the distributed Profinet IO to see when i have one of module in error/ not communicating i have try to use PNIODIAG but no succes. does somebody use function for TIA ? Thank you in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/31/2018 2:49:55 PMNew subject after splitting |
|
1/31/2018 7:34 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, check the answer of our Expert hdhosseini: |
Follow us on