2/5/2018 7:30 AM | |
Joined: 6/21/2006 Last visit: 7/6/2023 Posts: 21 Rating: (0) |
Dear Mr Denilson I have a question regarding the calibration procedure. In my application there is a tank which will be filed with chemicals. I want to measure the weight of these chemicals. So the load cell will have the weight of the tank and the weight of the chemicals inside it. During calibration the tank will be empty but the load cells will measure the weight of the tank. How will i be able to calibrate and set the weight to zero and then put a known weight and calibrate with it etc? I look forward to hearing from you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/5/2018 2:52:39 PMNew subject after splitting |
|
3/12/2018 1:05 PM | |
Joined: 1/4/2007 Last visit: 6/10/2024 Posts: 1129 Rating: (174)
|
Hello OIL&GAS, Which Siwarex module do you have? Best regards Siwarexi |
Follow us on