2/15/2018 12:02 AM | |
Joined: 1/12/2018 Last visit: 9/4/2024 Posts: 16 Rating: (0) |
Hello I have a turning machine with sinumerik 840D days ago the machine works well, but suddenly the control get disconnected, the procedure we made is, turn off the machine to do the procedure to delete the PLC and upload to the machine, it procedure works but if we turn off the machine, when we turn it on the PLC starts in STOP and we have to do the same procedure to upload a backup to the PLC We don't know why this happen, battery was changed and actually is new but just the PLC won't start after a complete shutdown and this the reason we have to execute the procedure of delete and upload the PLC. Does anybody know why happen this? best regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/15/2018 9:55:41 AMNew subject after splitting Last edited by: A_leX at: 2/15/2018 2:10:39 PM |
|
2/15/2018 2:13 PM | |
Joined: 1/12/2018 Last visit: 9/4/2024 Posts: 16 Rating: (0) |
The number in display is 6 but the leds of SF and BF is in red and selector S3 and S4 both are in 0 |
2/15/2018 2:34 PM | |
Posts: 531 Rating: (34) |
Is it a 840D or 840Dsl? Do you have a network connected to the x130 side? 840Dsl might help the lldp protocoll to be deselected. |
2/15/2018 3:09 PM | |
Joined: 1/12/2018 Last visit: 9/4/2024 Posts: 16 Rating: (0) |
Sinumerik we have is 840D power line |
Follow us on