3/16/2018 4:46 AM | |
Posts: 1 Rating: (0) |
Downloaded the upgrade as I already had V8.0 loaded form CD. I am able to go online from PC to 0BA8 and in the download window can get the online test to work successfully. When I click the refresh button it shows the network properties of the 0BA8 but will not download the program to the LOGO. Anyway back to the upgrade. The download is defined as having no or without Java VM. When attempting to install or upgrade on laptop I have message "Windows error 216 occurred while loading the Java VM". Is there a solution for this as I can not perform the upgrade? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/16/2018 9:36:28 AMNew subject after splitting |
|
5/3/2018 8:56 AM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33425 Rating: (4148)
|
No Google? Windows error 216 occurred while loading the Java VM |
5/3/2018 9:30 AM | |
Joined: 12/18/2014 Last visit: 7/27/2024 Posts: 33425 Rating: (4148)
|
I just wanted to tell you that you can get some troubleshooting by using Google. |
1/11/2019 5:57 PM | |
Posts: 1 Rating: (0) |
HI You have Windows 32 bits but you want to install the 64-bit program or vice versa |
Follow us on