3/22/2018 1:26 PM | |
Posts: 12 Rating: (2) |
I need to create a user hmi interface where user can create, edit and save data into a database. One ingredients table, one recipes table with percent ingredients quantities, and an production order table width recipe quantity batches to produce. Can someone tell me if TIA is able to do the job? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/23/2018 10:59:15 AMNew subject after splitting |
|
3/26/2018 12:54 PM | |
Joined: 8/3/2009 Last visit: 11/15/2024 Posts: 14176 Rating: (1774)
|
Hello Miguel Tavares if you have a Runtime System like WinCC Advanced RT or WincC Professional RT you can use VB Script to connecto to an Database with ODBC Connection like this: https://support.industry.siemens.com/cs/ww/en/view/61883659 But on a WinCE Panel like Comfort Panels there is no possibility to connect with Database through VB Script. bye Murof |
If this Information really helps, you could use the Rate function |
|
4/28/2018 4:24 PM | |
Posts: 12 Rating: (2) |
Thanks, I will try that. But seems that Tia Portal is quite limited in this matter.... |
Follow us on