3/7/2018 10:54 PM | |
Posts: 10 Rating: (0) |
Hi, i understand fanuc has her own procedure to set up a CP, BUT for do so i need some Siemens information about the GSDML file: The CP i'm ussing is CP1604 v2.6. on hw config i'm abble to set up slot 1-16, where slot 1 is ussed for the CP communication. From this slot i need the moduleID (hexa number) and the subslotID (hexa number) for charge in my robot, this data is on GSDML file. I cant know for sure if the numbers who i ve picked up are ok. If there is someone who have faced this issue please let me know and tomorrow at the office i will upload the files and my numbers. Thanks in advance,
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/23/2018 2:43:21 PMNew subject after splitting |
|
5/10/2018 11:01 PM | |
Posts: 1 Rating: (0) |
I need to the same information! |
Follow us on