3/26/2018 1:05 PM | |
Posts: 101 Rating: (1) |
Hi Sir , I need other additional information: Normally I have to create a share folder which is the path of the target system on this PC ('server stabnd-by') whose project will be copied when I activate the command to load the project to OS (master) and OS (st- by)? + something else for confirmation, in session windows accounts/Pass must be always the same for all PCs (servers + clients)? thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/26/2018 7:35:54 PMNew subject after splitting |
|
3/29/2018 11:40 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (39)
|
Hello, you should use the WinCC project duplicator if i got you right. Regards |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on