4/3/2018 10:12 PM | |
Posts: 2826 Rating: (684) |
Configuration of homing: (Active and Passive configured in the same way) Application: Car moving on a track with one reference sensor at the reverse end of the track. There are three application positions: start, midway and end. STATEMENT: Passive homing does not work in Motion Control V6 (type: analog). Observation: The expected behavior from documentation reads: (see highlighted section in attachment)
Result ->
Three possibilities: (Siemens application example 109477583 was used as sanity check!)
|
Last edited by: #dP at: 4/3/2018 10:14:28 PM |
|
This contribution was helpful to1 thankful Users |
4/4/2018 9:54 AM | |
Posts: 2826 Rating: (684) |
Not relevant to the subject at hand. Attached active homing. |
4/4/2018 10:09 AM | |
Joined: 1/23/2013 Last visit: 8/10/2022 Posts: 226 Rating: (5) |
before executing MC_Home, I execute the MC_reset command |
Follow us on