4/24/2018 10:09 AM | |
Posts: 2 Rating: (0) |
Dear all, I use the Simatic Energy Manager Pro V7.0 Upd1 and WinCC RT Profesional V14 SP1, installed on a single PC. When I use EnMPRO --> Automatic acquisition -->Wizard --> Acquisition Wizard-->WinCC/PCS7--> I just read the database created in TIA V14 (Historical data) and not the tags created in this database. How can i do ?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/24/2018 12:35:31 PMNew subject after splitting |
|
5/22/2018 1:43 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8175 Rating: (169) |
New question published by Blumen22 is split to a separate thread with the subject How can use the "Additional Source Energy Manager Pro V7 Update 3". Best regards |
Last edited by: Jen_Moderator at: 5/23/2018 11:10:47 AMEdited subject. My Forum is the place to personalize your profile, |
|
Follow us on