5/2/2018 12:55 AM | |
Joined: 11/19/2015 Last visit: 6/13/2024 Posts: 4 Rating: (0) |
Hi guys, I have four s7 400H plc on same network (communicated with each other) and 4 HMI and One redundant Scada system. this system is running very well. IP address are 192.168.1.11 .........................192,168.1.131 But, now our system will connect to Honeywell DCS system through modbus TCP/IP, so the DCS guy is saying to change the ip address 10.0.1.11 ...................... this DCS will connect with our one cp 443- module could u pls suggest me what should i do. is it any way to change the ip address of one cp 443 only and other plc and cps address remain old ip. for your easy reference i have attached screen shot please reply as soon as possible i m very upset with this Please please please ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/2/2018 7:34:37 AMNew subject after splitting |
|
5/2/2018 7:36 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
Closed cause question posted twice.
|
My Forum is the place to personalize your profile, |
|
Follow us on