5/4/2018 9:56 PM | |
Posts: 1 Rating: (0) |
Hi, everybody. I need you help. I need to establish the communication between PCS7 AS (v9.0) and 314CPU (s7 v5.3). The 317 is a old PLC that I can't modificate the program because its from a different vendor. What I can do??? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/7/2018 6:46:44 AMNew subject after splitting |
|
5/5/2018 7:23 AM | |
Joined: 9/9/2015 Last visit: 10/10/2024 Posts: 728 Rating: (279) |
Hi, Do you have the archive? If i were you, i could integrate it into my multiproject and connect them by s7 connection. After you establish the communication,is it for read only? Or write as well ? Do you know what to read and where to read? When write do there provide you the interface for you to write? Both of the plc could not write the same IO together. If you doesnt have the program, cant modify or do not know how to modify the old vendor program, is it possible to ask them link the field devices separately to your system? Hope these questions help you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on