5/24/2018 6:47 AM | |
Posts: 1 Rating: (0) |
Hellow, Sir i have a question that my engineering server which is updated now to PCS 8.1 was slow now a days in the start it was very fast when we run the system after a power failure.Than i found that we need to remove some alarm logs file which continually increased in the system to make it faster for boot after a power failure so can anybody tell me the exact location of the file which is having these logs. And if i m wrong than please correct me and show me the right way to keep my server fast. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/24/2018 12:30:51 PMNew subject after splitting |
|
5/24/2018 1:44 PM | |
Joined: 3/14/2008 Last visit: 9/26/2024 Posts: 2098 Rating: (938)
|
Hi, You can find the files at the following path: [Multiproject name]\[Name of PC station]\wincproj\[Name of OS]\ArchiveManager. You can find the files for Alarmlogging, Taglogging fast and slow. Good luck |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on