8/4/2008 10:07 AM | |
Posts: 739 Rating: (55)
|
Here are a example for a 1000mbar blower P0003 = 3 (Expert mod3) set point e.g. P1080[0] = 18 (min.frequenz 18Hz) P1082[0] = 55 (max.frequenz 55Hz) 3. value Analoginput 1= terminal 3/4 pressure value e.g.0 ... 1000mbar, 4 ... 20mA Analoginput 1= 0 - 20mA per DIP Switch 1 ON P0756[0] =2 (current input1) P0757[0] = 4 P0758[0] = 0 P0759[0] = 20 P0760[0] = 100 P0761[0] = 4 4. set point the e.g. 1000mbar= 100% P2201[0] = % (100mbarequals 10%, 500mbar 50% .....) P2216 = 1 P2253[0] = 2224 5. PID-Controler P2200[0] = 1 P2251 = 0 (PID-main set point) P2253[0] = 2224 (connection of PID-setpoint) P2264[0] = 755.0 (connection ofPID-value) P2280 ~ 3 (kP) P2285 ~ 10 (TN)
For more technical consulting please contact the Technical Support for Automation & Drives SIEMENS AG Tel: +49 (0) 180 5050 222 Fax: +49 (0) 180 5050 223 Mail: adsupport@siemens.com |
This contribution was helpful to2 thankful Users |
3/22/2018 8:36 AM | |
Joined: 6/19/2017 Last visit: 5/24/2024 Posts: 8077 Rating: (165) |
New question published by dilip00288 is split to a separate thread with the subject Control the speed of motor by temperature. What is enter the parameter in VFD?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on