11/27/2018 12:47 PM | |
Joined: 8/3/2012 Last visit: 12/4/2023 Posts: 18 Rating:
|
Hi everyone, I have the same issue. Tia portal V15 update 3 running on a VM (VMware Player 14.2) and Windows 7. My phisical machine runs Win10. The system was working till a couple of months ago (last time I tried to connect to a phisical PLC). Now I am I/O checking a new plant. I can connect, I have an FC online or a Tag Table or anything else but after 20/40seconds it says "Connection Aborted". I tried another PLC, a new network cable, an other port... If I Ping I can't see any interruption but in any case, after 20/40 seconds connection aborts. I did not install any new software (Virtual machine in not connected to Internet so no automatic update). I have no firewall both in Virtual Machine and in phisical machine. I also tried to reinstall VMPlayer, to reset ethernet connection... always the same issue. Can anyone help me? EDIT: the only think I did was to use PLC SIM. Does it make some interface change that can gives this error? (PG-PC Interface is configured properly) ------------------------------------------------------------------------------------------ |
Last edited by: mik_INFYNITY at: 11/27/2018 3:42:51 PMLast edited by: Jen_Moderator at: 11/28/2018 8:33:39 AMNew subject after splitting Last edited by: mik_INFYNITY at: 11/28/2018 8:55:17 AM |
|
11/28/2018 9:07 AM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating:
|
Hi, please check the following FAQ: What should you watch out for when installing STEP 7 (TIA Portal) on a virtual machine?Regards, Towome |
|
|
This contribution was helpful to
2 thankful Users |
Follow us on