1/7/2019 2:29 AM | |
Joined: 12/2/2016 Last visit: 9/30/2023 Posts: 81 Rating: (1) |
when i meet the fault i click ok button, then open another dialog. |
Last edited by: volcanol at: 1/7/2019 2:32:28 AM |
|
1/7/2019 2:31 AM | |
Joined: 12/2/2016 Last visit: 9/30/2023 Posts: 81 Rating: (1) |
does any body have meet this fault. OS: Windows server 2003 PCS: PCS7 V7.1 SP3 |
1/7/2019 7:20 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Volcanol, can u upload your installed SIMATIC software? (Start-> siemens automation folder-> Inst. Softwares) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
1/8/2019 1:48 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear volcanol, Let me try to help, 1. try to check AMDBase.db in your project folder. All user projects in a multiproject should have a AMDBase.db. I have found this thread, hope it is helpful for you. danijel said:" I found solution of problem with Siemens Support. 2. To create support request from Siemens, click here. Create Request They will guide you a proper way of doing it. 3. If you would like to try it on your own, probably u can try to delete/modify the name see whether the system will generate a new one with 2019 timestamp. (Not Recommended doing so in real project) Hope this is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to4 thankful Users |
Follow us on