3/21/2019 8:25 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hi, you can also take a lookon the PNIODiag Package https://support.industry.siemens.com/cs/ww/en/view/98278878 Whixh PLC and which Engineering/HMI System do you use? Christoph |
This contribution was helpful to1 thankful Users |
3/21/2019 8:45 AM | |
Joined: 5/18/2018 Last visit: 4/8/2022 Posts: 24 Rating: (1) |
S7 1500 and Runtime Advance. Im trying to find out if there is an easy way to copy that topology overview to HMI. Its not even about diagnosis but all the connections and overview of network. It looks like there is no easy automatic way to generate that. |
3/21/2019 9:00 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hello, for S7-1500 you will find a example here: https://support.industry.siemens.com/cs/ww/en/view/68011497 Topology overview ist not so easy. The PLC can only detect the direct connected partner devices , a device behind a device can not direct checked from PLC. Here you need a full Offline Topology in the project for all components. Then you can check with the systemdiagnostics if all devices are ok and connected. A topology search online from PLC to evaluate which devices are connected to which port, which ports between devices and so on is not possible . Regards Christoph |
This contribution was helpful to2 thankful Users |
10/5/2019 5:19 PM | |
Posts: 2 Rating: (0) |
Thanks everyone. But I couldn't get what your solutions. Sounded complex. I need to use Topology to see the Drive component with number 11. I am new to Siemens Diagnostics. {snip} ...sent from App ----------------------------------------------- New question published by RapNumeric is split to a separate thread with the subject "fault cause 33". |
Last edited by: The Helping Hand at: 10/07/2019 10:54:31 |
|
Follow us on