5/10/2019 12:36 AM | |
Posts: 3 Rating: (0) |
for my endwork i want to make an automated bridge for that i will use a bosch rexroth servo that i will control via a S7-1200 i established a connection between the plc and the motor but i don't know how i have to control it ( starting the homing, enabling the drive, .....) i already had contact with people with people from bosch rexroth they helped me configure the motor but they didn't know how you could control the motor via a siemens plc. Can anyone help me out ? (links goes to my project) [snip] AttachmentGIP V2.zip (462 Downloads) |
Last edited by: Jen_Moderator at: 05/10/2019 10:52:53Removed link, because the file seemed to be unsave. Last edited by: Jen_Moderator at: 05/10/2019 12:43:45Sorry - Added Link as an attachment belated. |
|
5/10/2019 1:31 PM | |
Posts: 3 Rating: (0) |
i do it via profinet and i exchange 14 bytes |
5/10/2019 3:14 PM | |
Posts: 3 Rating: (0) |
i am using the function block but when i try jogging and drive enable nothing happens ( i am also using new value acceptance to start the jogging) i sometmes get error F4009 (bus failure) don't know if it wil help with anything [snip] AttachmentIndradrive Cs.zip (694 Downloads) |
Last edited by: Nick.Matthyssen at: 05/10/2019 15:21:50Last edited by: Jen_Moderator at: 05/13/2019 07:22:07Removed link and added file as an attachment. |
|
Follow us on