5/19/2019 9:36 PM | |
Joined: 11/6/2017 Last visit: 1/16/2023 Posts: 27 Rating: (1) |
Hello Everyone! I'm facing a problem regarding WinCC RT configuration file. Actually, I want to run the file independent from TIA Engineering but when clicking on pdata.fwc file it shows following error "the file format of the configuration file with the version 11.0.2.0 is incompatible with the installed runtime version 13.0.1.0, generate the configuration file with runtime version 13.0.1.0 again" Although, there is no issue while simulation from TIA engineering. I'm using TIA portal V13 with update 9. The HMI has also built in the same version. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/20/2019 07:33:21New subject after splitting |
|
5/21/2019 10:04 PM | |
Joined: 11/6/2017 Last visit: 1/16/2023 Posts: 27 Rating: (1) |
So nice of you for direction. The problem has been resolved. Thanks |
Follow us on