5/22/2019 10:23 AM | |
Joined: 7/2/2018 Last visit: 8/1/2024 Posts: 16 Rating: (1) |
-Operating System: - - TIA Version : TIA V15.0 - Service pack and update :TIA V15.0 - Hardware Modules numbers : Profinet, CPU315-2, ABB VFD driver - The desired application : Collect data from ABB VFD Driver to Siemens PLC - The Problems (Bugs) : Hi, I would like to read data from ABB VFD such as current, voltage, running hour and power consumption. 1. I have read a few stuff online (ABB website, gsd files, block FB500 as attached: https://library.e.abb.com/public/8e4a4a75677e4b04a828059e684a672a/ABB_Drives_function_blocks_for_Siemens_PLCs_Quick_start-up_guide_A_A4.pdf ) but its normally controlling the VFD. What if i want to collect data from the VFD? 2. I dont really understand the theory of telegram, control and status word. From what i learnt, Control word (Output to VFD) are output to VFD, speed control; while status word and process data (Input from VFD) got what difference? Do i need to use the ABB FB500 block or just read the parameter of hex address from the VFD. Correct if i am wrong. - Expected causes of the Problem : Able to collect data from ABB VFD Thank you in advanced. AttachmentABB_Drives_function_blocks_for_Siemens_PLCs_Quick_start-up_guide_A_A4.pdf (341 Downloads) |
Last edited by: Jen_Moderator at: 05/24/2019 07:54:25Added PDF as an attachment. |
|
Follow us on