6/18/2019 12:39 PM | |
Joined: 5/6/2010 Last visit: 5/5/2024 Posts: 1965 Rating: (272) |
Hello Dhafar, I wouldn't use resistors to reduce the voltage. The best way is to use a solid state relay to trancduce the voltage. e.g. from Phoenix Contact. Solid-state relay module - PLC-OPT- 24DC/TTL - 2900363 You need then also a DC/DC converter from 24 to 5 V DC eg. also from Phoenix Contact DC/DC converters - MINI-PS- 12- 24DC/ 5-15DC/2 - 2320018 Then you should have no problems with your interface at the stepper. regards |
Follow us on