10/10/2019 12:06 PM | |
Joined: 7/31/2019 Last visit: 2/16/2024 Posts: 6 Rating: (0) |
Hello, I seem to have a problem with the HMI Tag's Value Change -event in TIA Portal v15.1. If I assign an Edit Bit -function to be triggered by another tag's Value Change -event, it doesn't work. I've managed to get the value change event working only by assigning the tag to a switch element, but not with a button with Edit Bit -function of the same tag. It's hard to explain, but please see the pictures below so you might catch what I mean. In the first picture you can see how I've assigned the tags. The Switch -element and the button change the state of the "button" -tag, and the value change of this tag triggers Invert Bit of "bit". In Picture 2 I've pressed the switch, and you can see how the state of "button" changed to 1, as well as the "bit", triggered by the value change of "button". In Picture 3 I've pressed the button and the value of "button" changes to 1, but "bit" remains 0. I've tried rebuilding the project, removing the IM files, but nothing seems to fix this issue. I did the same program in TIA portal V15.0 and it seems to work, so might this be a glitch related only to v15.1? Attachmentpictures.zip (414 Downloads) |
Last edited by: The Helping Hand at: 10/10/2019 15:20:33Added pictures as attachment. |
|
10/10/2019 3:02 PM | |
Joined: 4/26/2012 Last visit: 6/3/2024 Posts: 1530 Rating: (162) |
You tried in the I / O field event.
|
"Always make a backup before and check the best time before testing." |
|
Follow us on