10/16/2019 1:24 PM | |
Posts: 80 Rating: (0) |
Hello all, I have different sensor types to connect to several Analog Input modules (AI 8xU/I/RTD/TC ST, 6ES7531-7KF00-0AB0). I intend to connect 2-wire, 3-wire and 4-wire sensorsto the same Analog Input Module but I see in TIA portal that I have to configure only one mode for the whole module. [snip] Second Question: why is it necessary, from the point of view of electronics, to configure this? I mean, I understand that what changes is the way I supply 24V to the transmitter, but this is external to the module itself, which should be able to receive 4-20 mA either way. Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/17/2019 10:58:59New subject after splitting. Division of questions into seperate topics. |
|
10/16/2019 6:37 PM | |
Posts: 80 Rating: (0) |
Thank you, thats exactly what I needed. [snip] |
Last edited by: Jen_Moderator at: 10/17/2019 11:01:13Division of answers into seperate topics. |
|
Follow us on