12/10/2019 4:13 PM | |
Joined: 4/17/2018 Last visit: 7/14/2024 Posts: 262 Rating:
|
Hello, Using TIA V16 on windows 7 sp1, I want to simulate Unified Compfort panel and after doing all steps as described in this link, I can see my project running in Simatic Runtime Manger but I can not simulate on google chrome, it tell me "this site is inaccessible" as you see in attachment So what could be the problem? |
12/16/2019 2:04 PM | |
Joined: 11/14/2018 Last visit: 10/31/2023 Posts: 502 Rating:
|
Hello Med_selmi, there is a FAQ regarding installation of WinCC Unified: Maybe with this you're able to check, if there is something else to be done to get simulation running. Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
This contribution was helpful to
1 thankful Users |
Follow us on