1/22/2020 11:05 AM | |
Joined: 9/8/2016 Last visit: 2/14/2024 Posts: 198 Rating: (10) |
Hi All, I have a project of WinCC (WinCC SimatiC Manager) in 7.4 version. What i would like to do is to upgrade WinCC project to the newest version of WinCC. For my knowledge the newest version of WinCC is v7.5 SP1 Upd01. My WinCC project has: - 1 WinCC Appl. objects, - 4 WinCC Appl. Client objects, - 3 WinCC Appl. Client Ref. objects, My questions: 1. How can i migrate my project? From my reaserch -> it is possible to migrate WinCC 7.4 to 7.5 SP1 Upd01 directly. But the question is how to make it from Simatic Step7? The only solution which in my opinion is to open project in WinCC 7.4 Explorer. Then S7 project data will be removed. Then migrate that project directly to WinCC 7.5.1.1. After this we can again integrate WinCC project with Simatic Manager. 2. What about licence? I try to find some information in "Migration of WinCC projects from V4 to V7". What new licences i should have? 3. What are "WinCC Appl. Client Ref." objects? I read a chapter about integrating WinCC with Simatic Manager from "WinCC - working with WinCC" manual but did not find answer why in my project are 3 WinCC Appl. Client Ref. objects. Attachment44029132_wincc_upgrade_v4_v7.5_en.pdf (622 Downloads) |
1/23/2020 8:33 AM | |
Joined: 9/8/2016 Last visit: 2/14/2024 Posts: 198 Rating: (10) |
Understood everything. Thank you. |
Follow us on