2/14/2020 1:13 PM | |
Posts: 2 Rating: (0) |
Is the CF card missing?? |
2/14/2020 3:41 PM | |
Joined: 10/11/2006 Last visit: 9/26/2024 Posts: 5907 Rating: (804)
|
Hello, I recommend to remove the CF card from the CU320-2 and then connect the CF card to the computer via a card reader. Then I would load a new firmware to the card. A description of how to update the firmware can be found at the following link under "Instructions to update the firmware of the SINAMICS S120 CU320-2 and CU310-2". https://support.industry.siemens.com/cs/ww/en/view/109762626 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
2/14/2020 4:39 PM | |
Posts: 4 Rating: (0) |
Thank you very much for your answer. I will try it ! Please I would like to know what can be the cause of this Problem ? |
Follow us on