3/9/2020 10:19 AM | |
Joined: 5/26/2011 Last visit: 8/5/2024 Posts: 456 Rating:
|
Good day experts! Quick question about SIWAREX U. I've read about manual and on some post here in the forum. I downloaded the sample project which uses the SIWA_FB. I think you can either get the weight value on the "GROSS_WEIGHT" (INTEGER) or "ADC_VALUE_FILTERED" (WORD). Can i input some range here (say my needed range is 0 kg to 50 kg? What would be the equivalent integer value on the 2 FB outputs above (something like 65535 or 32766?). Because I will need to convert the value to REAL to have it processed by program based on HMI values (compare into coils, etc.). Thanks a lot! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/09/2020 10:29:20New subject after splitting Last edited by: G_R_E_Y at: 03/09/2020 10:38:22Last edited by: G_R_E_Y at: 03/09/2020 10:39:44Last edited by: G_R_E_Y at: 03/09/2020 10:58:25 |
|
3/29/2020 6:49 AM | |
Joined: 5/26/2011 Last visit: 8/5/2024 Posts: 456 Rating:
|
By the way, since the weigh value is integer, does this mean the scale can only output a sensitivity of 1 kg (no 0.1)? |
Follow us on