3/24/2020 3:25 PM | |
Joined: 3/24/2020 Last visit: 10/5/2021 Posts: 6 Rating: (0) |
Okey, so what do I need to do? What is a panel image? How do I know if I installed it or not? Sorry! |
3/24/2020 3:35 PM | |
Joined: 4/24/2006 Last visit: 9/26/2024 Posts: 8742 Rating: (1168) |
Hello, The images are on a separate DVD. Or you can download from this link: SIMATIC STEP 7 incl. Safety and WinCC V16 TRIAL Download From TIA Portal v16, you need to install them separate. (Older versions did install the images automatically) Find the directory: C:\Program files\Siemens\Automation\Portal v16\Data\HMI\transfer\16\ Here you find the images. Best regards, Wizard |
This contribution was helpful to6 thankful Users |
11/10/2020 6:09 PM | |
Posts: 11 Rating: (0) |
Hello Wizard, I too am having this problem with portal V16. Somewhat of an inexperienced Siemens programmer here. At the location you described C:\Program files.......\transfer\16\, there are two zip files. SystemData.zip and WebContent.zip. If I just unzip those, will that "install" the images? Is there another step?? Thanks in advance. Mike C. |
11/10/2020 6:35 PM | |
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to5 thankful Users |
12/29/2020 7:24 PM | |
Posts: 10 Rating: (0) |
Still trying to figure out how to "install" these files. I download them, sure, then what? |
This contribution was helpful to1 thankful Users |
12/29/2020 7:47 PM | |||||||||
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello,
Comfort Panels, Comfort Panels Outdoor and Comfort Panels INOX
|
||||||||
Eng.Mohamed Ibrahim |
|||||||||
This contribution was helpful to7 thankful Users |
Follow us on