4/12/2020 9:20 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Hello everyone, I just found out something interesting which is SINEC PNI (Primary Initialization Network) We used to configure scalances using Primary Setup Tool from Siemens. Now, Siemens has announced a new open-source software named “SINEC PNI”, a successor of the PST which consists of more functionalities than PST. You may use this for
System Requirements
SINEC PNI Basic V1.0 Service Pack 1 Update 2 Software Download Attached with “SINEC PNI_R0.pdf” for a quick look. If you faced problem with PCAP driver, you may install it here. Hope this is something new to you guys . AttachmentSINEC PNI_R0.pdf (900 Downloads) |
Last edited by: JazTai at: 04/12/2020 09:22:18Last edited by: JazTai at: 02/25/2023 07:52:56Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
10/22/2020 4:19 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Check on the settings page in the second tab, you should select the correct network adapter (PG/PC interface) before you start scanning. I do not have experience in NCU, but I believed if you are able to ping, you should be able to use PNI to find it. If DCP (For profinet devices) is not working, try the key in the IP range and scan it. You may also upload a picture on the setting page for us to better understanding your problems. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on