5/21/2020 9:44 AM | |
Joined: 2/5/2013 Last visit: 10/15/2024 Posts: 321 Rating: (74) |
KTP 1200 Basic PN 6AV2 123-2MB03-0AX0 12.1'' TFT display, 1280 x 800 pixel, 64K colors; key and touch operation, 10 function keys; 1 x PROFINET, 1 x USB TP 1200 Comfort 6AV2 124-0MC01-0AX0 12.1'' TFT display, 1280 x 800 pixels, 16M colors; Touch screen; 1 x MPI/PROFIBUS DP, 1 x PROFINET/Industrial Ethernet interface with MRP and RT/IRT support (2 Ports); 2 x Multimedia card slot; 3 x US Hi h1ka2 Resolution is same for KTP1200 and TP 1200. KTP supports 10 function keys. If those keys assigned for particular operation in previous HMI program then before changing device to TP 1200 you need to check it. For TP 1200 you need below software package WinCC Comfort (TIA Portal) or WinCC Advanced (TIA Portal) or WinCC Professional (TIA Portal) It is not available for WinCC Basic (TIA Portal) Br, AmolG. |
Last edited by: AmolG at: 05/21/2020 09:52:02Please rate it. |
|
This contribution was helpful to1 thankful Users |
5/22/2020 7:06 AM | |
Posts: 3 Rating: (0) |
thank you
|
Follow us on