2/4/2021 2:08 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
there is no migration, only a simple open and that is it any screen of the errors available? |
2/10/2021 2:49 PM | |
Joined: 8/3/2017 Last visit: 4/11/2024 Posts: 142 Rating: (0) |
Anyone? |
2/10/2021 3:15 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
go to the project properties in Simatic Manager and search for the neccessary SW-packages. When the devices that are missing are Siemens devices, you can use the searchbar in the upper right here on this page. Type in the MLFB and search for downloads. I also recommend you to install the latest Hardware Support Package: STEP 7 V5.x Hardware Support Packages (HSPs - as at 01/2021) for installing hardware updates in the Hardware ConfigurationFor all not Siemens devices you need to contact the manufacurer of the device for a suitable GSD-file, that you can install. hope this helps, regards |
FCK WAR! |
|
Follow us on