6/1/2021 10:34 PM | |
Joined: 4/16/2021 Last visit: 2/23/2022 Posts: 33 Rating: (0) |
Hello please, from this exemple of Tala , you said that the parameter "PADR" has "F0F0" as a constant assigned to it.
how did you know ? ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 06/14/2021 10:19:48New subject after splitting; insert quote |
|
6/2/2021 2:46 AM | |
Joined: 10/7/2005 Last visit: 5/3/2024 Posts: 3004 Rating: (1046)
|
simply by looking at the S5 program that Tala provided in this thread in combination with the also provided info that FB203 (which has the parameter "PADR") is called from FB100. |
Cheers |
|
6/10/2021 3:13 PM | |
Joined: 4/16/2021 Last visit: 2/23/2022 Posts: 33 Rating: (0) |
Hello fritz , Can you explain to me how can you convert the absolue adress to a relative adress ? |
6/11/2021 2:18 AM | |
Joined: 10/7/2005 Last visit: 5/3/2024 Posts: 3004 Rating: (1046)
|
I haven't
Again I haven't and below is what I did say a few posts earlier in this thread: As for the absolute memory addresses, F0F1 is PY241 and EEFF is FY255 in your S5 942 CPU (see also attached extract from the 115U manual). Suggest you read this whole thread in peace again as the advice given to thread starter Tala back then also has the answers you are seeking |
Cheers |
|
Follow us on