12/12/2016 2:14 AM | |
Posts: 11 Rating: (0) |
Hello I think I've done complicated things with LOGO, but this apparent program is difficult I Need program with 3 input (pulse). (Example I1-10, I2-20, I3-30 seconds) Each entry corresponds to an OFF-delay time, in the Timer. If I do IN2 the off-delay is 20 seconds. But if the 20 seconds have not finished yet, and pressing I1 will add 10 seconds to the time remaining. So, each input add some time to the Timer Thanks Attachment3IN_timer_sum.zip (322 Downloads) |
12/14/2016 5:25 PM | |
Posts: 5225 Rating: (1185) |
Hi. Indeed a complicated challenge. It is not exactly what you are looking for because... The action of the output does however function as you wanted. But - I think this might give some ideas on what you can do. Helpful? AttachmentDesignIdea_Inputs add to time.zip (322 Downloads) |
12/14/2016 6:53 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32893 Rating: (4066)
|
Here is a possible solution from me. I assume that once the timer is controlled by an input, each additional input may only come once until the timer has expired. AttachmentAdd_times.zip (298 Downloads) |
Follow us on