7/6/2009 2:21 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi 1. Pictures and Tag are in WinCC separated. Your "PicWin1.Red" means the tag "Red" in the structure "PicWin1". And the attribut "TagPräfix" includes in the smallest way the structurname"PicWin1" as you did, but that was not your intension, rigth? What you need is something like hmiruntime.srceen(1).screenitem("PicWin1") ... (VB Script) With that you can change the properties of a picturewindow named "PicWin1"on the basescreen. What do you want to do with the tag, i do not understand. 2. Sorry you mixed to much. Your tag blue is a faceplate instance internal tag? What do you want to modify in the Faceplate from PLC ? Do you want to create in runtime interal tags? You creat in the tag management internal tags Please discribe what do you want to do, i have no idea regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
This contribution was helpful to
3 thankful Users |
7/9/2009 8:42 PM | |
Posts: 261 Rating:
|
Hi David4444, The "Picture Tree Manager" is used to manage a hierarchy of systems, subsystems and Graphics Designer pictures. You have to consider the following: · How to create and change the hierarchy of a project · How to define systems and subsystems · How to assign pictures to these systems · How to edit pictures · How to create containers For detail you may follow this link as well as the direct help options from wincc 6.0 or above. I can give you a simple process example. Say you are doing a Blast furnace project and you define your hierarchy as in ref_1 and actual HMI display in ref_2.
This is depending upon this followings · Working area · Button area Say your OS resolution is 1280*1024 and your start screen is @SCREEN.PDL. You will found the @SCREEN.PDL is fundamentally combination of followings: 1. @win11 picture window (1280*148) adapts picture @OVERVIEW1.PDL 2. @win13 picture window (1280*51) adapts picture @BUTTONS11.PDL 3. @win12 picture window (1280*825) adapts picture @1001.PDL Your basic screen size will be 1280*825. For detail you may follow this link as well as the direct help options from wincc 6.0 or above. best regards ddg Attachmentpic.zip (95 Downloads) |
This contribution was helpful to
3 thankful Users |
7/13/2009 1:59 PM | |
Joined: 6/2/2009 Last visit: 5/19/2024 Posts: 61 Rating:
|
Thank you for these precious precisions and information. Regards. David.
|
Follow us on