8/6/2009 5:02 AM | |
Posts: 10 Rating: (0) |
thank you |
8/7/2009 8:46 AM | |
Posts: 672 Rating: (57) |
Hi, You need to set output Q64.3 Most of us as plc programmers would put some hidden key press to get it to go true. If you have a copy of the plc program then look for the output and see what is driving it. An alternative is to set the value using the plc status display see attachment Attachmentstatus display.pdf (445 Downloads) |
This contribution was helpful to2 thankful Users |
8/7/2009 11:27 AM | |
Posts: 672 Rating: (57) |
Ha Ha, Took me a while to get an elg up and running correclty. Can't upload manual:- file too big can email if want |
8/8/2009 9:11 AM | |
Posts: 10 Rating: (0) |
thank you my email is fengxinwen01@163.COM |
8/12/2009 10:18 AM | |
Posts: 10 Rating: (0) |
There is no Q64.3 used in the PLC programe ,why? |
Follow us on