8/10/2010 7:05 AM | |
Posts: 9 Rating: (2) |
My system consist of S7-400 CPU.It is STEP 7(v5.4SP4)& WinCC(v7.0 SP1) project.I have used AS-OS engineering for creating tags using monitoring and control parameterand Alarm 8P(SFB35) block for generating Alarms.But I am facing problem in WinCC.Eventhough I have 2K WinCC RCLicense its giving error that license is running in demo mode and after some time it is showing license expired .I am attaching screenshots for reference.So can you please tell me what is the problem??? Which licenses we have to install while using AS-OS engineering feature for STEP7(v5.4 SP4)and WinCC(v7.0 SP1) project.
Attachmentscreenshots.zip (450 Downloads) |
8/10/2010 11:02 AM | |
Posts: 9 Rating: (2) |
Thanks Wizard. AttachmentLicense_log.pdf (212 Downloads) |
8/10/2010 1:12 PM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi Well tell if your project is PCS7 or Normal step7 and winCC If your project in normal WinCC and step7 then do the following follow the steps. I think it will solve your problem Have fun.. Attachmenti1.zip (440 Downloads) |
Jazz |
|
This contribution was helpful to1 thankful Users |
8/11/2010 5:26 AM | |
Posts: 9 Rating: (2) |
Dear Tagolover only STEP 7 and WinCC are installed in system.It already STEP 7 project. |
8/11/2010 8:44 AM | |
Posts: 9 Rating: (2) |
Thank you all.My problem is solved.There was issue with the wincc project. |
This contribution was helpful to2 thankful Users |
11/23/2010 6:23 PM | |
Posts: 48 Rating: (0) |
Thanks you, It is ok now. Regards Marian |
Follow us on