Industry Online Support
Technical Forum
8/11/2010 2:24 PM | |
Posts: 5822 Rating: (412)
|
Hello Joakim, do you already know if the device you use supports the function: Replace device without interchangeable medium? If not, maybe check with your distributor or check the FAQ: Which PROFINET nodes support automatic commissioning and the replace device without interchangeable medium function? Using this feature would solve your issue. Sadly is a direct write request to store the Device name to "some" device over Ethernet MAC not known to me. To do so you wither need STEP7 or the PST Tool. Best regards J_Bell |
Follow us on