10/16/2010 1:56 AM | |
Joined: 10/7/2005 Last visit: 9/12/2024 Posts: 3020 Rating:
|
Hello dzordzo |
Cheers |
|
This contribution was helpful to
1 thankful Users |
10/16/2010 7:48 PM | |
Posts: 947 Rating:
|
Hello dzordzo need info from daig. bufferbefore event 7. It's you can attach in zip. it would be nice, if the archive were diagnostic buffers both CPU. I see part daig. buffer from CPU1, and not see Event occurred in the in rack 0. After restart cpu0 mustsynchronize their diag/ buffer with CPU1. This is strange. Perhaps this is due to an error memory submodule in CPU1, which was spoken of in the previous post fritz. Where the program is loaded from the ram-card or flash? You have entered a cold or warm restart? |
1/29/2018 10:31 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by MOHANMOLLI is split to a separate thread with the subject S7 417 4H redundant CPU's. recently it is taking too much time to go online . Best regards |
Follow us on