12/3/2010 5:50 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello, For sure CP5613 works with newer version of Intouch and SImaticNet via DA Server. In your case with using COM L S7 9 (it's a very old story) check Upgrading to SIMATIC NET CD 07/2001 or higher with existing S7 connections (created with COML S7) and Configuring an S7 connection under COM L S7 best regards, Hristo Mihalev |
12/3/2010 6:54 PM | |
Posts: 99 Rating: (0) |
thanks UMENCHO, the CP i am using is CP5613-A2. do you think it will work. the version of intouch i have is old in order to install the new the CP card and work as well, i installed simatic net version 6.2 / 2003 can you explain me about COM L S7 9? thanks again |
12/3/2010 8:12 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Creating a Database Using COML S7 (without "9"). The COML S7 program creates the .txt and .ldb files necessary for Simatic Net to interface the Siemens CP5613 card to either the MPI port on the S7-CPU, or the Profibus port. There exist one technote document regards establishing the connnection. the title is Tech Note 220. At the moment I don't have it, but if you couldn't find it in GOOGLE i can send you. BUT you have newer CP. (A2). In this case COM L S7 is not valid. This is part from older SimaticNet. The only way is to use OPC SimaticNet server (make PC Station and using OPC Scout to read from S7 CPU) and then using OPCLink to connect the data with Intouch. 1. Wonderware OPCLink User's Guide 2. How do you configure an S7 connection for a user application via PROFIBUS with the SIMATIC NET PC software? (this is also J_Bell' idea for S7 project). best regards, Hristo Mihalev Attachment220.pdf (380 Downloads) |
Last edited by: UMENCHO at: 12/3/2010 8:13 PMAaa found technote 220. |
|
12/3/2010 8:31 PM | |
Posts: 99 Rating: (0) |
thanks if i fallow what is mentioned in step 2, will it be enugh or i need to do both of them |
Follow us on