1/12/2011 11:04 AM | |
Joined: 6/7/2010 Last visit: 2/3/2023 Posts: 569 Rating: (37) |
Hi DigitalMD, I 802C the above said parameter is avaliable. Pls removeif any filter setting of parameter is done & check once. For your reference i have attached that (802C) machine data. 11300 JOG_INC_MODE_LEVELTRIGGRD 1: Jog mode for JOG-INC and reference point approachJOG-INC:When the traversing key is pressed in the required direction (e.g. +), theaxis begins to traverse the set increment. If the key is released before theincrement has been completely the traversed, the movement is interrupted andthe axis stops. If the same key is pressed again, the axis completes theremaining distance-to-go until this is 0. 0: Continuous operation for JOG-INC and reference point approachJOG-INC:When the traversing key is pressed (first rising edge) the axis travels thewhole set increment. If the same key is pressed again (second rising edge)before the axis has completed traversing the increment, the movement isaborted, i.e. not complete Attachmentmachine data.pdf (362 Downloads) |
Regards, |
|
1/14/2011 8:00 AM | |
Posts: 2964 Rating: (481)
|
Hi... Have you wired the Z axis reference CAM input properly could you check the same.... Also could you check the parameter 14512[17] bit 0/1/2 I am attaching you the Description of PLC Subroutine Library for SINUMERIK 802S/C base line Check it out.... AttachmentPLC_appl_Program.pdf (388 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on