3/8/2011 10:24 AM | |
Posts: 1064 Rating: (72) |
on the tp177a turn on switch 4 and turn off switch 1 see if that makes a difference . switch 1 is for plc and switch 4 is for pc |
3/8/2011 2:37 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi TelmeX, Here is link to manual and there ispage116 (3.13.1) andpage 401-402- transfering. http://support.automation.siemens.com/WW/view/en/18796010 Here is also link to help programming http://support.automation.siemens.com/WW/view/en/18660846 1. Check if there is right settings in your panel also 2. Compile your project and there can be warnigs, but not any errors! 3.Somethimeshave to Update the operating system on the HMI device first,then it´s possible to download project. page409 (19.2.3 Updating the operating system)
|
Last edited by: Heksu at: 3/8/2011 3:31 PMLast edited by: Heksu at: 3/8/2011 2:58 PM"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
Follow us on