5/11/2011 1:22 PM | |
Joined: 4/23/2009 Last visit: 1/24/2024 Posts: 7 Rating: (0) |
Dear All, Need urgent help to open the protool project created with v1.x I tried to open it with v6.0 i am getting this error. " The project was created with protool version 1.X. In protool version 2.0 and later project are stored in single file. The directory having the project name is no longer required." I check this thread also /tf/WW/en/Posts/51253#top But problemstill exist. Protool Project file which i have iswith no extension & required .pdb file to open it also not present. Please can any one have an idea to open protool project created with v1.x ?? |
5/11/2011 1:36 PM | |
Joined: 4/29/2010 Last visit: 7/15/2024 Posts: 1557 Rating: (161)
|
Hello, check this faq in this case: Open Pro Tool 1.x configuration with current software best regards |
This contribution was helpful to1 thankful Users |
5/12/2011 10:50 AM | |
Joined: 4/29/2010 Last visit: 7/15/2024 Posts: 1557 Rating: (161)
|
What kind of file do you allready have if it isn`t a PDB. best regards |
5/12/2011 11:38 AM | |
Joined: 4/23/2009 Last visit: 1/24/2024 Posts: 7 Rating: (0) |
Hi Sandman, I have attached the file which i am trying to open. This is the only file i have. I tried with adding .PDB extension to this file & open with Protool 6.0 but its not working. Please if you get any idea tell me. Thanks, Amir Attachmentnitrogenop17.zip (1179 Downloads) |
6/19/2015 1:06 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
|
Follow us on