6/7/2011 10:07 AM | |
Joined: 4/29/2010 Last visit: 8/8/2024 Posts: 1557 Rating: (161)
|
Hello, if you don`t knew the password the only thing to remove this password is to reset the panel (os-update). But have you allready try the password "100" (default password)? Take a look at this faq for the reset of the panel: How do you do an operating system update (OS update) on operator panels? If you do a reset to factory settings you don`t need to enter the transfer settings in the panel. best regards. |
3/16/2018 9:11 AM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating: (169) |
New question published by Naveen Paliwal is split to a separate thread with the subject Remove Password From (Control Panel) MP277 10'' . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on